Popular hero

The orange is pretty hard to miss. And yet the vertical stripes have precisely the opposite effect. They help this little cinema hero to hide from enemies. Because he secretes a slime on his skin, he is protected from the poison of sea anemones, which allows him to hide among them. So predators go away with nothing. This creature, which lives in the Indian and Pacific Oceans and is threatened with extinction, can live for up to ten years. More than 30 different types live in the oceans and only a few of them are orange. But the type in question obviously makes us laugh – as its name suggests.

 

What creature are we talking about?